4.0.0
Embedded Inference Client ST Edge AI Client APIs (Application Example)


ST Edge AI Core

Embedded Inference Client ST Edge AI Client APIs (Application Example)


ST Edge AI Core Technology 4.0.0




Introduction

This article includes a complete reference snippet related to the usage of the ST Edge AI Embedded Client APIs

/**
  ******************************************************************************
  * @file    stai_main_app.c
  * @author  AST Embedded Analytics Research Platform
  * @date    2024-05-23T10:34:45+0200
  ******************************************************************************
  * Copyright (c) 2024 STMicroelectronics.
  * All rights reserved.
  *
  * This software is licensed under terms that can be found in the LICENSE file
  * in the root directory of this software component.
  * If no LICENSE file comes with this software, it is provided AS-IS.
  ******************************************************************************
  */
#include <inttypes.h>
#include <stdio.h>
#include <string.h>

#include "stai.h"             /* include ST Edge AI macros, types and data structures */
#include "network_inputs.h"   /* where input1 buffer is defined */
#include "network.h"          /* include ST Edge AI generated network model */


#define LOG_PRINT(fmt, ...) \
  { printf(fmt, ##__VA_ARGS__); fflush(stdout); }


int main(int argc, char* argv[])
{
  stai_return_code return_code = STAI_SUCCESS;

  LOG_PRINT("name:%s\n", STAI_NETWORK_MODEL_NAME)

  LOG_PRINT("n_inputs:%d\n", STAI_NETWORK_IN_NUM)
  LOG_PRINT("n_outputs:%d\n", STAI_NETWORK_OUT_NUM)

  LOG_PRINT("activations:%d\n", STAI_NETWORK_ACTIVATIONS_SIZE_BYTES)
  LOG_PRINT("weights:%d\n", STAI_NETWORK_WEIGHTS_SIZE_BYTES)
  LOG_PRINT("runtime_name:STM.AI\n")

  /*  !New!: Declare and allocate memory for private network context instance */
  STAI_NETWORK_CONTEXT_DECLARE(network, STAI_NETWORK_CONTEXT_SIZE)

  /* !New!: Runtime initialization */
  return_code = stai_runtime_init();

  /*  Initialize network context  */
  return_code = stai_network_init(network);
  if (return_code != STAI_SUCCESS) {
    LOG_PRINT("  ## Test Failed executing stai init: 0x%x.\n\n", return_code)
    return -1;
  }

  /*  Declare activations buffer pointers array  */
  stai_ptr activation_buffers[STAI_NETWORK_ACTIVATIONS_NUM] = {0};

  /*  Allocate and set activation buffer #1  */
  STAI_ALIGNED(STAI_NETWORK_ACTIVATION_1_ALIGNMENT)
  uint8_t activation1[STAI_NETWORK_ACTIVATION_1_SIZE] = {0};
  activation_buffers[0] = (stai_ptr)(activation1);

  /*  Allocate and set activation buffer #2  */
  STAI_ALIGNED(STAI_NETWORK_ACTIVATION_2_ALIGNMENT)
  uint8_t activation2[STAI_NETWORK_ACTIVATION_2_SIZE] = {0};
  activation_buffers[1] = (stai_ptr)(activation2);

  /*  !New!: Set network activations buffers  */
  return_code = stai_network_set_activations(network, activation_buffers, STAI_NETWORK_ACTIVATIONS_NUM);
  if (return_code != STAI_SUCCESS) {
    LOG_PRINT("  ## Test Failed executing stai set activations: 0x%x.\n\n", return_code)
    return -1;
  }

#if 0
  /* NOTE: This step is no more required now in ST Edge AI Client APIs since weights buffers are generated and bind 
     directly to the C model */
  /*  !New!: Declare activations buffer pointers array  */
  stai_ptr weight_buffers[STAI_NETWORK_WEIGHTS_NUM] = {0};
  stai_size n_weights = 0;
  return_code = stai_network_get_weights(network, weight_buffers, &n_weights);
  if ((return_code == STAI_SUCCESS) && (n_weights==STAI_NETWORK_WEIGHTS_NUM)) {
    return_code = stai_network_set_weights(network, weight_buffers, n_weights);
  } else {
    LOG_PRINT("  ## Test Failed executing stai set weights: 0x%x.\n\n", return_code)
    return -1;
  }
#endif

  /* Inputs Buffer Setup */
  /* C-Table declaring inputs buffer pointers array and set inputs addresses */
  stai_ptr input_buffers[STAI_NETWORK_IN_NUM] = {
    (stai_ptr)input1 /* defined in network_inputs.h */
  };

  /*  !New!: Set network inputs buffers  */
  return_code = stai_network_set_inputs(network, input_buffers, STAI_NETWORK_IN_NUM);
  if (return_code != STAI_SUCCESS) {
    LOG_PRINT("  ## Test Failed executing stai set inputs: 0x%x.\n\n", return_code)
    return -1;
  }

  /* Outputs Buffers Setup */
  /*  Allocate and declare output buffer #1  */
  STAI_ALIGNED(STAI_NETWORK_OUT_1_ALIGNMENT)
  float output1[STAI_NETWORK_OUT_1_SIZE];
  
  /*  Declare outputs buffer pointers array and set outputs addresses */
  stai_ptr output_buffers[STAI_NETWORK_OUT_NUM] = {
    (stai_ptr)output1
  };

  /*  Set network outputs buffers  */
  return_code = stai_network_set_outputs(network, output_buffers, STAI_NETWORK_OUT_NUM);
  if (return_code != STAI_SUCCESS) {
    LOG_PRINT("  ## Test Failed executing stai set outputs: 0x%x.\n\n", return_code)
    return -1;
  }

  stai_network_info info;
  return_code = stai_network_get_info(network, &info);
  if (return_code != STAI_SUCCESS) {
    LOG_PRINT("  ## Test Failed executing stai get network info: 0x%x.\n\n", return_code)
    return -1;
  }

  LOG_PRINT("* Runtime version   : %d.%d.%d\n",
    info.runtime_version.major, info.runtime_version.minor, info.runtime_version.micro)
  LOG_PRINT("* Tool version      : %d.%d.%d\n",
    info.tool_version.major, info.tool_version.minor, info.tool_version.micro)
  LOG_PRINT("* APIs version      : %d.%d.%d\n",
    info.api_version.major, info.api_version.minor, info.api_version.micro)
  LOG_PRINT("* Network nodes     : %d\n", info.n_nodes)
  LOG_PRINT("* Network macc      : %d\n", info.n_macc)
  LOG_PRINT("* Network inputs    : %d\n", info.n_inputs)
  LOG_PRINT("* Network outputs   : %d\n", info.n_outputs)

  /*  Execute network model inference on sample test (synchronous mode)  */
  LOG_PRINT("Starting inference\n")

  /* The run API now supports both sync and async modes */
  return_code = stai_network_run(network, STAI_MODE_SYNC);

  LOG_PRINT("Completed inference\n")
  if (return_code != STAI_SUCCESS) {
    LOG_PRINT("  ## Test Failed executing stai network run: 0x%x.\n\n", return_code)
    return -1;
  }

  LOG_PRINT("__START_OUTPUT1 __\n")
  for(int32_t o = 0; o < STAI_NETWORK_OUT_1_SIZE; o++) {
    const float value = ((float*)output1)[o];
    if (o != 0 && o % 10 == 0) {
      LOG_PRINT("\n")
    }
    LOG_PRINT("%f " ", value);
  }
  LOG_PRINT("\n__END_OUTPUT1 __\n")

  /*  Network de-initialization  */
  return_code = stai_network_deinit(network);

  /* Runtime de-initialization */
  return_code = stai_runtime_deinit();

  return (return_code == STAI_SUCCESS) ? 0 : -1;
}