ST Edge AI Core - Modular installer
ST Edge AI Core Technology 4.0.0
r1.1
Overview
The 'stedgeai-<osname>-onlineinstaller'
application is a console utility and graphical user interface to
install the different components of ST Edge AI Core. It offers the
possibility to install the components needed for the selected
targets. This tool allows also to create offline installers with the
selected components for future usage on a machine not connected to
the internet.
A 'maintenancetool' is automatically generated in
the installation to add, update or remove components. The tool is
based on QT
Installer framework. If the installation directory is not owned
by an administrator account, the installation can be done without
administrative rights. If you want to install in a common system
place, then administrative rights are required for the
installation.
Supported '<osname>' name:
windows, linux, mac or
macarm
Available components
The modular installer comes with one component per target and dependencies on hidden components
| Component | Description | Dependencies | Supported Operating Systems |
|---|---|---|---|
| stedgeai0105.base | common components for all targets (hidden) | Windows, Linux, Mac, MacArm | |
| stedgeai0105.core | common components for STM32, STELLAR and ISPU targets (hidden) | stedgeai0105.base | Windows, Linux, Mac, MacArm |
| stedgeai0105.stm32mcu | STM32Cube.AI component targeting all STM32 MCUs | stedgeai0105.core stedgeai0105.stm32mculib | Windows, Linux, Mac, MacArm |
| stedgeai0105.stm32mculib | STM32Cube.AI inference libraries for the STM32 MCUs (hidden) | OS independent | |
| stedgeai0105.stneuralart | STNeural-Art component targeting STM32N6 with Neural Art | stedgeai0105.stm32mcu | Windows, Linux, Mac, MacArm |
| stedgeai0105.stm32mpu | STM32AI-MPU component targeting STM32 MPUs | stedgeai0105.core | Linux |
| stedgeai0105.stellarmcu | StellarStudio.AI component targeting STELLAR MCUs | stedgeai0105.core stedgeai0105.stellarmculib | Windows |
| stedgeai0105.stellarmculib | StellarStudio.AI inference libraries for the STELLAR MCUs (hidden) | OS independent | |
| stedgeai0105.ispu | ISPU.AI component targeting sensors with an ISPU core | stedgeai0105.core | Windows, Linux, Mac, MacArm |
| stedgeai0105.mlc | MLC.AI component targeting sensors with an embedded machine learning core | stedgeai0105.base | Windows, Linux, Mac, MacArm |
Graphical User Interface installation
For graphical user interface based installation just double click on the stedgeai-osname-onlineinstaller command, select the installation directory, select the components to install, accept the license terms, optionally select the start menu shortcut and launch the installation.
Command line installation
Synopsis
Only the significant subset of options is displayed below, please refer to the QT Installer framework documentation for the full set of options
Usage: stedgeai-<osname>-onlineinstaller [options] command <args> <key=value>
Commands:
in, install - install default or selected packages and aliases - <pkg|alias ...>
ch, check-updates - show available updates information on maintenance tool
up, update - update all or selected packages - <pkg ...>
rm, remove - uninstall packages and their child components - <pkg ...>
li, list - list currently installed packages - <regexp for pkg>
se, search - search available aliases or packages - <regexp for pkg|alias>
Note: The --filter-packages option can be used to specify additional filters for the search operation
Note: The --type option can be used to specify the content type to search
co, create-offline - create offline installer from selected packages - <pkg ...>
cc, clear-cache - clear contents of the local metadata cache
pr, purge - uninstall all packages and remove entire program directory
Options:
-?, -h, --help Displays help on commandline options.
--help-all Displays help, including generic Qt options.
-v, --version Displays version information.
-d, --verbose Verbose mode. Prints out more
information. Adding -d or
--verbose more than once
increases verbosity.
--sp, --system-proxy Use system proxy on Windows
and Linux. This option has no
effect on macOS. (Default)
--np, --no-proxy Do not use system proxy.
--su, --start-updater Start application in updater
mode. This will override the
internal marker that is used to
distinguish which kind of
binary is currently running.
-t, --root <directory> [CLI] Set installation root
directory.
--oi, --offline-installer-name <filename> [CLI] Set custom filename for
the generated offline
installer. Without this the
original filename is used with
an added "_offline-yyyy-MM-dd"
suffix.
--ns, --no-size-checking Disable checking of free space
for installation target.
--fp, --filter-packages <element=regex,...> [CLI] Comma separated list of
additional key-value pair
filters used to query packages
with the search command. The
keys can be any of the possible
package information elements,
like "DisplayName" and
"Description".
--cp, --cache-path <path> Sets the path used for local
metadata cache. The path must
be writable by the current
user.
--type <package|alias> [CLI] Sets the type of the
given arguments for commands
supporting multiple argument
types, like "search". By
default aliases are searched
first, and if no matching
aliases are found, then
packages are searched with the
same search pattern.
--am, --accept-messages [CLI] Accepts all message
queries without user input.
--rm, --reject-messages [CLI] Rejects all message
queries without user input.
--da, --default-answer [CLI] Automatically answers to
message queries with their
default values.
--al, --accept-licenses [CLI] Accepts all licenses
without user input.
-c, --confirm-command [CLI] Confirms starting of
installation, update or removal
of components without user
input.
--mco, --max-concurrent-operations <threads> Specifies the maximum number
of threads used to perform
concurrent operations in the
unpacking phase of components.
Set to a positive number, or 0
(default) to let the
application determine the ideal
thread count from the amount of
logical processor cores in the
system.
Arguments:
Command Command to be run by
installer. Note that this
feature may be disabled by
vendor.
Args Extra arguments for command,
each separated by space.
InstallerValue Key-value pair to be set
internally by the framework.Creating an offline installer
From the provided online installer tool, you can create an offline installer tool using the following command. The offline creation tool will automatically download the selected components and the associated components dependencies.
The offline installer tool can be used can be used graphically or by command line. In command line mode the same arguments as described above can be used.
stedgeai-<osname>-onlineinstaller create-offline [packages]
for example
./stedgeai-windows-onlineinstaller --root C:/tmp/stedgeai --offline-installer-name stedgeai-windows-offline create-offline stedgeai.stm32mcuInstallation maintenance
After installation, at the root of the installation directory, a
'maintancetool' is created
The maintancetool can be used graphically or by command line with the same arguments as the installation tool
With the maintenance tool you can
- Add or remove components
- Update components to a newer version
- Remove all components (uninstallation)
When a component is installed using the offline installer the maintenance tool can only be used for uninstallation of the package.
For the online version, it will query the online repository for the available versions and propose an upgrade of the installed components.