On-target STELLAR validation flow
for STELLAR target, based on ST Edge AI Core Technology 4.0.0
r2.2
Overview
This article describes the process to build a Stellar Studio
SDK-based AI validation firmware including the deployed model and
the aiValidation stack.
The AI validation firmware is used by the stedgeai application ('validate --target sr5[xx] (or sr6p[xx] or or sr6g[xx]) -mode target'
command) to perform the on-target validation.
After that the build process has been completed, using one of the
compilers supported in the Stellar Studio Stellar-E or Stellar P/G
SDK, the next step is to flash and run the AI validation firmware on
the Stellar-E or Stellar-P or Stellar-G target.
The flashing of the Stellar-E or Stellar P/G AI validation firmware
can be done using one of avaiable debugger/programmers available for
the Stellar devices, like OpenOCD SW and StellarLink USB dongle (if
the HW is not already present in the Stellar evaluation
board).
For OpenOCD, it’s automatically added when installing Stellar
Studio: under the openocd/docs folder you can find a guide
on “How to use OpenOCD and StellarLINK in
StellarStudio”.
You can also find under openocd/scripts some utilities and
documents on how erase and flash Stellar programs.
For StellaLink USB dongle, you can find sw drivers under the
openocd/drivers folder but you also refer to “StellarLINK
in-circuit debugger/programmer for Stellar and SPC5 automotive
microcontrollers” and “StellarLINK
device drivers”.
Please refer to “User manual - Getting started with Stellar Studio AI plugin for Artificial Intelligence (AI)”, “AI commands” section to have a complete overview of the Stellar Studio AI plugin (based on the ST Edge AI Core) and of the full process to validate a model on the target.