4.0.0
Use USB-CDC device driver for validation


ST Edge AI Core

Use USB-CDC device driver for validation


for STM32 target, based on ST Edge AI Core Technology 4.0.0



r1.1

Purpose

This article is a how-to to explain how to enable the USB-CDC profile to perform faster the validation on the board. A client USB device with the STM32 Communication Device Class (i.e. Virtual COM Port) is used as communication link with the host. It allows to avoid the overhead of the ST Link bridge connecting the UART pins to/from the ST Link USB port. However, a STM32 Nucleo or Discovery board with a built-in USB device peripheral is requested.

Note

This how-to is illustrated with a Nucleo H743ZI, but all STM32 development board with a built-in USB device peripheral can be used. The associated USB driver (including its USB-CDC middleware) is used w/o modification, setting or debug of this stack is out of this article.

Project creation

To create a firmware with the USB CDC driver, a standard project should be created with the USB stack enabled, including the USB Device middleware with the Communication Device Class (Virtual Port Com). Default options are used. For the AI part, the core and validation application should be selected (refer to [UM]). IDE project should be generated (automatic validation on target feature is not supported).

The generated IDE project is ready to be used. Before to compile the project, the following adaptations are requested to use the USB-CDC client drivers:

Optionally, the default size of the USB RX and TX buffers can be reduced to limit the usage of the RAM (USB_DEVICE/App/usbd_cdc_if.h file)

#define APP_RX_DATA_SIZE  64  /* instead 2048 */
#define APP_TX_DATA_SIZE  64  /* instead 2048 */

Validation on target

After this adaptation phase of the code, the firmware is generated and flashed on the board. During the initialization of the firmware, a phase of enumeration is performed with the host to discover the profile and to create a virtual com port. Name and value of this new COM port is system dependent. In this example, the new COM port appears as COM8 (Windows® 10 environment).

Normal validation on the board can be executed, through the UI (Baudrate value is not considered)

or through the command line

$ stm32ai validate -m <model_file> --target stm32 --mode target -d COM8

Performance improvement

With a Nucleo H743ZI board (@96MHz) and a typical floating-point model (--full option and a batch of 100 samples are used).

Used COM port execution time
ST Link + baudrate 115200 27s
ST Link + baudrate 921600 14,4s
USB-CDC full speed 8.7s