Release Note
ST Edge AI Core Technology 4.0.0
Overview
Part of the ST Edge AI Suite (https://www.st.com/content/st_com/en/st-edge-ai-suite.html), the ‘stedgeai’ application is a console utility that provides a complete and unified Command Line Interface (CLI) to compile a pretrained DL/ML model into an optimized library. This library can run on an ST device or target, enabling edge AI on MCUs, MPUs, and smart sensors.
This article documents the main feature changes, interface changes, and reported defects that have been fixed. Check the STMicroelectronics support website at www.st.com/content/st_com/en/st-edge-ai-suite.html for the latest version.
Release v4.0.0
Main changes
- Added support for ISPU target on IIS3DWB10IS sensor.
- ISPU target now requires ISPU toolchain 1.5.0 or newer, based on the stred-gcc compiler. For older versions of the toolchain use ST Edge AI Core 3.0.0.
- Added support for the Stellar SR6 P3E line automotive integration MCU. The Neural-ART support is not available.
- Added support for STM32U3 series, including the Hardware Signal Processing (HSP) unit.
- Added support for STM32V8 series based on the Arm® Cortex® M85 core including Arm® Helium™ technology.
- No critical API break/change
Upcoming removals
- Suport to Larq layers is marked as DEPRECATED, it will be removed in the next release (no replacement).
- Support to Keras Lambda layers is marked as DEPRECATED, it will be removed in the next release (no replacement).
- The old embedded inference client API or legacy API is marked as DEPRECATED. It is no longer maintained and will be removed in a future release. It is replaced by the. It is replaced by the stai API.
Enhancements and new features
- Improve the check and associated error message for invalid arguments, including invalid combinations and unused arguments for a given target or command.
- Initial improvement of the execution time of the STEdgeAI Core CLI
- Improve support to models with int64 tensors
- Improve constant propagation optimization
- New layers:
- ADD_N (TFLite)
- LayerNormalization (Keras)
- LayerNormalization (ONNX)
- Size (ONNX)
- STELLAR target
- Added the sr6p3e new target
- Move from Stellar P&G SDK v5.1.0 to v5.2.0
- Validation on target on sr6p3e R52 cores
- Stellar Studio AI plugin v4.0.0 updated accordingly
- STM32 target
- Runtime loadable model support for Neural-ART
- Improve and align the callback interface with LL ATON files
- Enhance checking of invalid clang relocation
- Add support for model without parameters
- Runtime loadable model support for Neural-ART
- Neural-ART/NPU target
- Improve SWISH recognition. Automatically done for version with alpha == 1.0 and intermediate values quantized. Added option --SWISH-recognition to recognize SWISH with alpha != 1.0 and ignoring intermediate quantization.
- Add recognition of expanded scale/offset GELU using tanh option.
- Add option --expand-softmax to enable expansion of softmax layer in a set of layers that are mappable in hardware. The expansion may cause small loss in precision the mapped networks generated with this option should be tested carefully.
- Enable by default clone_dma; deprecated
--Oclone-dmaoption and added new option to disable optimization (--Ono-clone-dma). - Added new option --ec-optimize to enable epoch controller blobs optimizations to be considered experimental generated code needs to be tested for loss of precision.
- Extend deadlock removal for multiple deadlock cycles ending on same node.
- Increase the rate of HW managed convs having constrained batch = 1 and features 1x1.
- Disable depthwise inflation for non-expanded scale offset conv that will be managed in SW.
- Add new backward-range-estimation heuristic to select
significant bits in expanded scale-offset convolution. It can
positively impact the accuracy when the accumulation ranges have
high variance. It can be enabled with dedicated option
--backward-range-estimationand it’s designed for advanced users that can evaluate the related accuracy impact. - Optimize channel-broadcasted access for arithmetic operations having both non-constant inputs.
- Add int8 SW fallback for TILE and GATHER.
- Recognize patterns convertible to POW with second input constant map it on activation interpolator scale/offset pow by a constant
- New STEdgeAI CLI option to enable use of epoch-controller at
top-level (
--enable-epoch-controller)
Reported defect fixes
- Fixed support to ONNX 1D ConvTranspose (AIAFF-931)
- Fixed support to ONNX EinSum (AIAFF-230)
- Fixed support to ONNX models with “array” or “t_out” string in tensor names
- Fixed support to per-tensor TFLite PReLU
- Fixed Digital MAC signature issue (AIEAC-336)
- Fixed NPU inference time issue in 3.0 - 2.2 regression - (AIAFF-1632)
- ISPU target
- Fixed possible issue with validation on target with NUCLEO-U575ZI-Q just after flashing the firmware.
- MLC target
- Fixed initial windows skipping during features generation not being applied when filters are used.
- Fixed comments about operation types in generated headers.
- Neural-ART target
- Fixed LL runtime compilation issue for Zephyr environment (AIEAC-321)
- Fixed crash with fp32 runtime loadable model (AIEAC-236)
- Fixed corner case of pooling layer when input tensor quantized with an offset different from 0.
- Fixes regarding debug information in generated info json file.
- Bugfix matmul expansion: Handle separately h and w axis indexes for A, B, and output.
Known limitations
- STELLAR target
- The generated Neon runtime library relies only on compiler options: it lacks optimization code with intrinsic SIMD instructions
- The sr6p3e neural art processing support is not available
Runtime
- LL_ATON
- Few cleanups and fixes in relocatable code
Documentation
- Updated articles related to Stellar targets.
- Remove the articles/sections relating to the X-CUBE-AI plug-ins
CLI and API Changes
- The
--quantizeargument is removed. Only self-contained quantized model files are supported. Proprietary support for quantized models through a specific JSON file is removed. The proprietary support of the quantized model through specific json file is removed. - STM32 target
- Add –hsp option to enable the support of the Hardware Signal Processing (HSP) unit for STM32U3 series
- Removed the unused
--ihexargument. In relocatable mode, the--addressargument instructs directly the code generator to produce an additional binary file in Intel Hexadecimal Object File Format only. - Built-in test application for STM32N6 series - cycles required to prepare the input and output buffers before calling the inference are excluded from the measured inference time.
- ISPU target
- Added mandatory
--deviceargument to specify the name of the sensor embedding the ISPU to target. - Removed
--ucfargument (previously deprecated). Use--ispu-confinstead.
- Added mandatory
- STELLAR target
- Added option
--target sr6p3eto support the new sr6p3e target.
- Added option
Embedded C-api
- No API breaking change
Release v3.0.0
Main changes
- Embedded inference
ST-AI API is now the default generated API.
- legacy API generation is still available via --c-api option.
- Support of all available SR5/SR6 family devices from SDKs: sr5e1, sr6p3, sr6p6, sr6p7, sr6g6, sr6g7, sr6p7g7
- Runtime loadable model generation for ST Neural ART is available via CLI (-r/--relocatable option extension).
- If the --json-val
option is not used, validation results are saved in a new JSON file:
<network>_c_info_valid.json. - For the Neural-ART support, the default C-name is aligned to the
standard ST Edge AI Core naming (
networkinsteadDefault). - Added support to 4-bit weights (8 bits activations) of Convolution and Dense Layer, natively on Neural-ART and with int8-bit fallback on SW targets.
- stm32mp target support removed. Use ST Edge AI Core 2.2 instead.
Enhancements and new features
- Update ONNX from 1.15.0 to 1.16.2
- Update ONNX runtime from 1.18.1 to 1.19.2
- Added constant propagation for Reduce 1D and max layer
- Added support to single entry SoftMax
- Added the computation of the Signal to noise ratio (SNR) metric
- Added support to ONNX-ML LinearRegressor
- Forced ONNX runtime to use reference kernels
- STELLAR target
- Refactoring of target device information
- Target device CLI option with new set of aliases based on the SR5/SR6 family devices
- Automatic Build generation of Stellar components
- Move from Stellar P&G SDK v4.4.1 to v5.1.0
- Move from Stellar E SDK E v1.9.0 to v1.10.0
- Support of the GNU Arm embedded 13.3.1-2024.06 toolchain version
- Update default API type from legacy to st-ai
- Validation on target on R52 cores and execution of AI applications based on new st-ai
- Stellar Studio AI plugin v3.0.0 updated accordingly
- STM32 target
- Added in the CLI the support for runtime loadable model generation (relocatable mode) for Neural ART runtime
- Extended built-in validation environment to support multiple runtime loadable models
- Neural-ART/NPU target
- Zephyr support: Illustrated by the Zephyr Computer Vision application: https://github.com/stm32-hotspot/zephyr-stm32n6-ai-people-detection
- Major improvements in activation mapping, buffer management,
hardware/platform support, and code quality
- Refined buffer allocator logic, bandwidth estimation, and live range handling. Compared to the version 2.2, requested memory usage may be slightly different in certain corner cases.
- Enhanced support for relocatable models and cache coherency
- Improve support of the following operators
- Quantized TFLite: COS (HW), COSH (HW), ELU (HW), EXP (HW), REDUCE_MIN (HW), REDUC_MAX (HW), SIN (HW), ARG_MAX (SW_INT), ARG_MIN (SW_INT)
- QDQ ONNX: ArgMax (SW_INT), ArgMin (SW_INT), BatchNormalization (HW), Elu (HW), Reciprocal (HW), ReduceMin (HW), Selu (HW)
- exported Pytorch GELU operator (expanded with ONNX opertors including the Erf operator, ‘tanh’ approximation is not supported). ONNX Gelu operator is not supported.
- initial support of Swish/SiLU operations.
Reported defect fixes
- Fixed support to custom layers in Keras3 models
- Fixed accuracy issue of PReLU mapped on Neural-ART
- Fixed support to models with repeated output
- Fixed support to MatMul layer in some corner cases
- Fixed support to LSTM layer in some corner cases
- Fixed support to int64 indices in Slice layer
- MLC target
- Fixed external sensitivity for LSM6DSV320X
- Fixed 256 g full scale for ISM6HG256X
- Fixed MLC source registers address in the output metadata for LIS2DUX12, LIS2DUXS12, and IIS2DULPX
- STM32N6 validation stack
- Fixed IO buffer allocation (alignment of MCU cache line)
Known limitations
- STELLAR target
- The generated Neon runtime library relies only on compiler options: it lacks optimization code with intrinsic SIMD instructions
Runtime
- Add new library variant (COMPATIBLE version) for Arm® Cortex® M55 (STM32N6 series). Compiled with MDK Arm Compiler v6, it can be in GCC or IAR application environment (approximately 10–20% faster execution time).
Documentation
- Added Neural-ART article about the deployment/management of the memory initializers
- Update the “How to upgrade a STM32 project” article to add the detailled information about the used ARM embednet toolchain to generate the network runtime libraries.
- Remove article related to the TensorFlow Lite support for Microcontroller.
CLI and API Changes
- Neural-ART/NPU target
- The
--mveiNPU compiler option is removed. The NPU compiler ‘–load-cdesc’ option specifies the specific MCU/host configuration. This option is automatically added by the ST Edge AI Core derived from the --target option.
- The
- The
--allocate-inputs/outputsoptions are deprecated (default behavior). To avoid the allocation in the activations buffer, the –no-input/ouput-allocate options should be used. - STM32 target
- The
--no-c-filesoption is removed. By default, for the relocatable mode, the associated C-files are not generated. Extra reloc parameter (gen-c-files) can be used.
- The
Embedded C-api
- No API breaking change
Release v2.2.0
Enhancements and new features
- Fixed limitation about the Keras 3 models generated with the Sequential API
- STELLAR target
- Full support for stellar-pg devices
- Arm® Cortex® R52 with NEON extensions (SIMD, dual precision floating-point) network runtime libraries added
- Validation on target enabled for the Arm® Cortex® R52 cores with NEON extensions
- Stellar Studio AI plugin v2.2.0 updated accordingly
- Stellar Studio AI demos added to run inferences on different stellar-pg devices and cores
- Full support for stellar-pg devices
- ST Neural-ART NPU target (stm32n6 + ST Neural-ART NPU)
- Add new N6 validation project configuration (usbc support)
- Add new N6 validation project for Arm®
Cortex® M55 core only
- Add Nucleo-boards support for both validation projects
- N6_scripts:
- Add a
--cleanoption to then6_loader.pyto clean the validation project before building - Add a new
cm55_loader.pyscript to ease loading of the CM55 validation project on stm32n6 - Enhance logging (log files are more verbose than before)
- Add a
- Enhance NPU support for runtime loadable model
(relocatable model) - Python scripts v1.3
- Support for LLVM-based toolchain environment
- Add option to put the ecblobs (const data part) with params/weights
- Allow absolute @ for external memory pool (activations)
- NPU compiler
- Added HW support for Scale-Offset Max, Min, Neg operations
- Runtime
- Introduced
ll_aton_rt_user_api.has the main user API include. IntroducedLL_ATON_RT_SetNetworkCallbackand deprecatedLL_ATON_RT_SetEpochCallback.
- Introduced
- STM32MPU target
- Re-enable support after backend
update/alignment.
- Re-enable support after backend
update/alignment.
- ISPU target
- Improved memory occupation and execution time of the pattern
Convolutional layer + Non-Linearity + Pooling for int8 quantized
models
- Improved execution time of Max pooling layers in int8 quantized models
- Improved execution time of Convolutional layers with per channel quantization
- Improved execution time of Convolutional / Dense layers in int8 quantized models
- Improved memory occupation and execution time of the pattern
Convolutional layer + Non-Linearity + Pooling for int8 quantized
models
Reported defect fixes
- ST Neural-ART NPU target (stm32n6 + ST Neural-ART NPU)
- Fixed unresolved symbols during the generation of the
relocatable model
- Fixed compilation warnings during the RT runtime computation when RELATIVE address mode is used for a given memory-pool
- NPU compiler
- Fixed various clang-tidy warnings and code style issues.
- Fixed bugs in scale/offset computations, kernel value estimates, and quantization propagation.
- Addressed issues with ECasm, ECtracer, and ECloader regarding encryption, patches, and relocations.
- Fixed problems with batch2output mode of concats and min/max kernel estimates.
- Corrected handling of less-than-8-bits initializers and quantization for unit tests.
- Fixed error handling and improved assertion usage (converted asserts to ATONN_ASSERT or exceptions).
- Fixed unresolved symbols during the generation of the
relocatable model
- MLC target
- Fixed missing high-g accelerometer power down at the start of generated configuration
- Fixed issue with parsing of datalogs with single column
- Fixed parsing of “ext_x”, “ext_y” and “ext_z” columns in datalogs
- Fixed vAFE usage for ST1VAFE6AX
- Fixed supported MLC ODRs for ST1VAFE3BX
- Fixed feature names and sensitiviy parsing in vAFE only mode for ST1VAFE3BX
- Fixed crash on invalid feature type
- Fixed crashes when using the maximum or almost the maximum number of features
- ISPU target
- Fixed wrong Batch_Normalization float parameters merge into Convolutional layers with ONNX QdQ int8 models
Known limitations
- Caution AiRunner package associated
communication protocol has changed:
- Newer versions of AiRunner will not work with older validation projects
- Newer validation project will not work with older AiRunner versions
Documentation
- ST Neural-ART NPU target (stm32n8 + ST Neural-ART NPU)
- “How to update my project with a new version of ST Edge AI Core?” (new article)
- Update the “Runtime loadable model support” article.
CLI
- Add option to set parametric dimensions in the shapes of the input tensors.
- Add option to enable an ONNX simplifier pass before to import the ONN model.
Embedded C-api
- no API breaking change.
- The embedded inference client API (legacy) will be marked as DEPRECATED.
Release v2.1.0
Enhancements and new features
- Add support for Keras 3 models (.h5 and .keras);
back-compatibility to Keras 2 model has been maintained.
- Add support for Keras 3 ops: absolute, arccos, arccosh, arcsin, arcsinh, arctan, arctan2, arctanh, argmax, argmin, ceil, cos, cosh, divide, equal, erf, floor, floor_divide, greater, greater_equal, hard_silu, leaky_relu, less, less_equal, log, logical_and, logical_not, logical_or, logical_xor, maximum, minimum, mod, negative, not_equal, relu, relu6, round, rsqrt, selu, sign, sin, sqrt, tan, tanh
- Update Keras from 2.15 to 3.7.0
- Update TensorFlow from 2.15.1 to 2.18.0
- New layers:
- ATAN2 (TFLite)
- SCATTER_ND (TFLite)
- ScatterND (ONNX)
- SIGN (TFLite)
- ISPU target
- Add support for sensor configuration in JSON file format for validation on target
- Add self-sufficient validation on target mode (does not require the generation step and the build of the validation application for ISPU)
- Solved long time for board auto-discovery when performing validation on target on some setups
- Improved performance of int8 multi-channel dense layers
- MLC target
- Add support for new MLC-compatible devices (IIS2DULPX, LSM6DSV80X, ISM6HG256X, LSM6SDV320X)
- Improve ProfiMEMS board data injection functionalities for accelerometer devices
- Add support for the new ProfiMEMS board STEVAL-MKI109D
- Add full support for sensor configuration in JSON file format
and remove support for UCF file format
- Generate command now creates the sensor configuration in the JSON file format and the new header file formats (regular and minimal)
- Validate command now accepts the argument
--mlc-confto provide a sensor configuration exclusively in JSON format
- Solved long time for board auto-discovery when performing validation on target on some setups
- Stellar target
- Support for stellar-pg target
(SR6P line - 32-bit Arm® Cortex® M4 automotive integration MCUs for
dme and dsph cores)
- Arm® Cortex® M4 network runtime libraries for GCC GNU, HIGHTEC
and ARCLANG Arm compilers with FPU support enabled (single
precision)
- Validation on target not enabled for Arm® Cortex® M4 cores: only available for Arm® Cortex® R52+ cores
- Switch to the new official generated json file
(c_info.json)
- Stellar Studio AI plugin v2.1.0 updated accordingly
- Stellar Studio AI multicore demo added to run multiple NN on
both R52+ and M4 cores
- Arm® Cortex® M4 network runtime libraries for GCC GNU, HIGHTEC
and ARCLANG Arm compilers with FPU support enabled (single
precision)
- Support for stellar-pg target
(SR6P line - 32-bit Arm® Cortex® M4 automotive integration MCUs for
dme and dsph cores)
- STM32 target
- Add support for stm32u3
series.
- Add support for stm32u3
series.
- ST Neural-ART NPU support
- Add script/guideline to profile a deployed model
- Add support to generate a runtime loadable model (relocatable model)
- Add a toolsuite to support encrypted-weights
inference
- New features
- ReduceMean Support: Implemented support for ReduceMean and other Reduce* nodes.
- Swish Activation Detection: Added peephole for Swish activation detection, optimizing models like YOLO and EfficientNet.
- Encryption Support: Introduced encrypted
weights and decryption nodes in the epoch controller.
- Performance improvements
- Optimized cache maintenance and memory pool handling.
- Improved hardware mapping for edge cases and extended support
for broadcasting eligibility.
- Optimized cache maintenance and memory pool handling.
- Bug fixes
- Fixed memory pool alignment issues.
- Resolved bugs in Stream Engine limit computation and DMA address
limit configuration.
- Addressed compiler warnings and undefined behavior in arithmetic lowering.
- Fixed JSON output generation and node mapping issues.
- Fixed mapping and allocation issues for epoch controller parameters.
- Add script/guideline to profile a deployed model
Known limitations
Keras 3 models generated with the Sequential API (
Sequential class) are not fully supported. It is recommended to use the Model or Functional API to design models. A workaround to import this type of model with the ST Edge AI Core is to convert it to a TFLite model.converter = tf.lite.TFLiteConverter.from_keras_model(loaded_model) tflite_model_f32 = converter.convert() with open(TFLITE_FILE, 'wb') as f: f.write(tflite_model_f32)STM32MPU target
- Not supported with STEdgeAI Core 2.1 for compatibility reason (STEdgeAI Core 2.1 should be used)
Documentation
- new articles about the ST Neural-ART NPU to support a relocatable mode and to explain how to profile a deployed model.
- new article about weights encryption support on ST Neural-ART NPU
- new article about the code generation output report “c_info.json”
CLI
- no API breaking change
--fulloption is marked as DEPRECATED. It will be removed in the next release.
Embedded C-api
- no API breaking change
- The embedded inference
client API (legacy) will be marked as
DEPRECATED.
- Default value for the
--c-apioption will change in the next release to be set tost-ai. - '
legacy' c-api will be always available but will no longer be fully tested or maintained in the future release. - It is recommended to use the new c-api.
- Default value for the
Reported defect fixes
- Removal of an installed component does not require anymore removal of the corresponding directory
- Different bugs related to import of TFLite BATCH_MATMUL and ONNX Gemm/MatMul have been fixed
Release v2.0.0
Enhancements and new features
- Update ONNX version from 1.10.2 to 1.15.0
- Update ONNX runtime package from 1.17.3 to 1.18.1
- New layers:
- BATCH_MATMUL (TFLite)
- BROADCAST_ARGS (TFLite)
- BROADCAST_TO (TFLite)
- GATHER_ND (TFLite)
- GatherND (ONNX)
- RELU_0_TO_1 (TFLite)
- Layer extensions: MatMul with >2D inputs
- Extend ‘validate’ flow to create different numpy npy files by
input/output for original model and deployed c-model.
- CLI options
- Add
--input-memory-alignmentand--output-memory-alignmentto control I/O memory alignment
- Improve options to control the data layout for input
and output tensors (that is, channel position):
--inputs-ch-positionand--outputs-ch-positionwhich replaces--input-output-channel-position - Introduce
-–cut-input-tensors,--cut-output-tensors,--cut-input-layers,--cut-output-layersoptions to cut the model before starting the analysis
- Add
- Support for STM32N6 series, including the ST Neural-ART
accelarator™
- Arm® Cortex® M55 network runtime libraries with NVE support enabled (GCC GNU Arm, IAR, Keil® AC6 toolchains)
- Support for stellar-pg target
(SR6P line - 32-bit Arm® Cortex® R52+ automotive integration MCUs,
Arm v8-R compliant)
- Arm® Cortex® R52+ network runtime libraries for GCC GNU and HIGHTEC Arm compilers with FPU support enabled (single precision)
- Stellar Studio AI plugin v2.0.0 updated with the Stellar SR6P3
support
- Stellar Studio AI SR6P3 demo added to perform the on-target
validation
- Developer Cloud extension updated with the support of the
SR6PX-EVBC4000P (Rev. A) board for the SR6P3
- Extend support for stm32mp25 target
- Add validate command for validation on target
- Add
--entropyoption for generate command to convert on-the-fly per-channel quantized model to per-tensor quantized model (this can impact accuracy).
- Add
--input-data-typeand--output-data-typeoptions for generate command to force the generated model to interpret inputs/outputs as float32 instead of float16 (these variables can only be used when the provided model has FLOAT32 inputs/outputs). - Improve support for ONNX models
- Add individual nodes execution-time measurement when performing
validation on target for ISPU
- New firmware and template from GitHub (https://github.com/STMicroelectronics/st-mems-ispu) are necessary
- Native support for QKeras 16-bits fixed-point quantization schemes for ISPU target (dense, convolutional, and ReLU layers)
- Extend MLC validation on target datalog formats to support all ST MEMS software for logging data (MEMS-Studio, Unico-GUI, Unicleo-GUI, and ST AIoT Craft)
- Add default behavior to MLC validation on target if
LABEL_{N}ground truth column is missing for decision treeDT_{N}: metrics computation is replaced with predicted class frequency counts. - Add support for new MLC-capable devices (ASM330LHBG1, ST1VAFE3BX).
Documentation
- Update Stellar articles to be more generic regarding the family devices supported
- Update the Command Line Interface article to add the stellar-pg target
- Stellar Studio AI user manual - Getting started with Stellar
Studio AI plugin for artificial intelligence (AI) updated
- Create a HowTo article to explain how to use the AiRunner package
- Provide a set of new articles about the ST Neural-ART accelarator™
- Enrich ISPU articles with additional details regarding generated code integration and validation on target
- Add new article with definitions, gloassary and trademark
- MLC device-specific documentation for newly added devices (ASM330LHBG1, ST1VAFE3BX)
Interface changes
CLI
--allocate-inputsand--allocate-outputsoptions are deprecated. This is now the default behavior of the CLI. The new options:--no-inputs-allocationand--no-outputs-allocationcan be now used to avoid to request the allocation of the inputs/outputs buffers in the activations buffer.
--input-output-channel-positionis removed. Replaced by--inputs-ch-positionand--outputs-ch-positionoptions.
Embedded C-api
- no API breaking change
Reported defect fixes
- Fix support to models with constant outputs
- Fix support ONNX QdQ ConvTranspose
- Fix computation of shapes for some layers
- Fix optimizations of quantized convolution models
- Fix support to quantized GEMM through floating-point fallback
- Fix import of ONNX QdQ models with unsigned input
- Fix possible issues when a workspace populated by previous releases is used
- Fix generated network details data structure partially allocated in data RAM
- Fix fallback to float approximation error for 16-bits QKeras models
- Fix C implementation selection for validation on host with target ISPU in some specific cases
- Fix convolutional layers C implementation mapping when number of kernels >= 8 for ISPU target
Limitations
- When one installed component is removed you need to manually remove the directory with the component name in the Utilities/<osname>/targets directory. For example if you remove the mlc component in the installation, you need to manually remove the Utilities/<osname>/targets/mlc directory.
Release v1.0.0
Initial release of the ST Edge AI Core technology. It introduces the support of the new ST devices: MCU, MPU, and smart sensors and a flexible installer to install only the requested components for a given target.
Enhancements and new features
Initial release.
Interface changes
No changes.
Reported defect fixes
Initial release.
Previous releases
What is new in X-Cube-AI V9.0.0?
Enhancements and new features
- CLI
- core is now based on a new executable (
'stedgeai') targetting different ST devices. The underlying technology and asociated flows (analyze,generateandvalidate) are similar to the previous version, only some options have been harmonized. It introduces a new embedded C-API:st-ai, not yet documented allowing to unify the interface and providing a relative more simple C-interface. - the “quantize” command has been removed. Note that the quantized models through the tensorflow, ONNX, qKeras or Larq are always supported (see [QUANT][X_CUBE_AI_QUANT] article)
- core is now based on a new executable (
- new operators
- ConvTranspose (KERAS)
- NOT_EQUAL, GELU, ZEROS_LIKE (TFLite)
- quantized 8b UNIDIRECTIONAL_SEQUENCE_LSTM (TFLite)
- Mod (ONNX)
- Core - Code generator
- introduce new embedded C-API (experimental), option
'--c-api st-ai'should be used.
- introduce new embedded C-API (experimental), option
- Embedded Library
- bz167868 - remove usage of the CRC IP to lock the network-runtime library
- bz154982 - optimize implementation of the quantized dense layers
- bz157480, bz154026, bz161225, bz167236, bz162208 - multiple optimizations for quantized PW/DW layers
- bz146681 - enhance LSTM support for quantized 8b version (TFLite operator)
Major bug fixes
- (bz161128) fix wrong zeropoint sign mgt in SUB operation with scalar as second operand
- (bz160077) fix to support multiple input tensors produced by a same operator
- (bz164547) fix the merge of the BN in dense layer
- (bz164479) fix code generator with Conv1D and stride = 2
- (bz160262) fix internal shape computation for ONNX flatten operator
What is new in X-Cube-AI V8.1.0?
Enhancements and new features
- UI
- add specifix checkbox allowing to set the “–no-onnx-io-transpose” option
- include new version of [TensorFlow Lite for Microcontrollers][X_CUBE_AI_TFLM] (SHA-1 : 6a1803)
- CLI
- enhance global model format detection, improve the report of the number of operation per layer
- Core - Code generator
- optimization of the quantized kernel implementations: CONV2D (bz151774), ADD (bz153931)
- add support for new layers:
- Einsum (bz121864), BitShift / ONNX Operators
- Support to the gather with second input variable (TFLITE & ONNX Operators)
- Support to LSTM with constant inputs not put in initializers (bz141640)
- Embedded Inference API
- no new features
Major bug fixes
- (bz129411) TFLITE - support for transpose of batch dimension
- (bz152744) ONNX - enhance import of concat operator managing arbitrary inputs order
- (bz148917) ONNX - enhance import of resize operator considering the constant inputs
- (bz135654) TFLITE - enhance Dilated convolution 1D/2D (SpaceToBatchNd/BatchToSpaceNd)
- (bz141553) ONNX - support transpose lop between dequantize and convolution ops
- (bz144706) run-time lib - extend n_macc resolution to 64b
- (bz149752, bz150344) code gen - memory allocator, enhance multiple heap support
What is new in X-Cube-AI V8.0.0?
Enhancements and new features
- CLI
- for a given model, the
analyzeandgeneratecommands report the [requested memory size][CLI_ref_requested_memory_size] (FLASH and RAM) for the deployed AI stack (infrastructure + used kernels)
- Relocatable mode - Initial support for [Custom layers][X_CUBE_AI_KERAS_CUSTOM], only self-containts custom c-files.
- (bz138721) - relocatable mode - API files
(
ai_reloc_network.c./.h) are exported in the bundle of the generated files.
- for a given model, the
- Core - Code generator
- (bz111201) ONNX - add support for [quantized ONNX models][X_CUBE_AI_QUANT] (QDQ format)
- (bz135734) ONNX - add scalar tensors support
- (bz136311) DQNN - improve support to hybrid int1/int8
convolution
- Upgrade ONNX runtime module to 1.13.1 version (ONNX 1.10.2 version is not upgraded), allowing QDQ support
- (bz136824) KERAS - support to StridedSlice in Keras TFOpLambda/Lambda Layer
- add support for new layers:
- QLinearMul (ONNX QOperator)
- (bz136250) Renderer - improve concat deployment
- Embedded Inference API
- (bz112264) Align with CMSIS 5.9
- Embedded documentation
- add [new article][X_CUBE_AI_QUANT] to describe the support of the quantized models. It provides the guidelines/options/limitations to quantize a TensorFlow and ONNX model.
- STM.AI “quantize” is marked as deprecated
Major bug fixes
- (bz113917) ONNX - channel first layer with constant eltwise input
- (bz138240) TFLITE - support of pad on channel dimension
- (bz139113) KERAS - fix import of the 4D placeholders
- (bz136824) KERAS - support to lambda layer with closure
- (bz135790) STM32 test app - fix compilation warnings when -pedantic option is used
What is new in X-Cube-AI V7.3.0?
Enhancements and new features
- User Interface
- upgrade the support of the [TensorFlow lite for microcontroller
runtime][X_CUBE_AI_TFLM]
- add optional selector to define the objective of the optimizations
- upgrade the support of the [TensorFlow lite for microcontroller
runtime][X_CUBE_AI_TFLM]
- CLI
- add global optimize option to enable or not the optimization
passes to tend to reduce the requested RAM size or to minimize the
inference time (or latency) (see
[
'-O/--optimization'][CLI_optimization_option] option) - cli:reloc - use the ISO C99 dialect to compile the c-files
(
'-std=c99'option)
- add global optimize option to enable or not the optimization
passes to tend to reduce the requested RAM size or to minimize the
inference time (or latency) (see
[
- Core - Code generator
- (bz133234) ONNX import - support model with input fixed shape and output with undefined shape
Major bug fixes
- (bz133214) CLI - improve log of the “generate” command.
'-v 2'option can be used to have more details about the imported/generated model.
- (bz133045) CLI - ai runtime library files from the user
workspace are not systematically updated between two “valid”
command.
- (bz133810) CLI - memory-pool - fix INTERNAL ERROR when requested RAM don’t fit in memory-pools.
- (bz131095) stm32 app - fix compilation warning with IAR
9.x
- (bz131121) stm32 app - fix HAL support for STM32MP1
- (bz131254) stm32 app - fix support for STM32C0 series
- (bz133743) code gen/runtime - fix support of concat with large
number of inputs
- (bz133783) code gen/runtime - fix Softmax on non-axis
channel
- (bz132916) DQNN / Larq - fix computation of the quantized
weights
- (bz133202) Fix regression when a BN is folded in a DW
layer
- (bz132508) GUI - restore correct “Allocate Inputs/Outputs”
check-boxe values between two sessions
- (bz131253) GUI - fix display of the available external SDRAM for
STM32F469i board
- (bz134118) GUI - fix validation on target for STM32U5 series
What is new in X-Cube-AI V7.2.0?
Enhancements and new features
- User Interface
- TensorFlow lite for microcontroller is always based on the code
available in 7.1 release
- unify and centralized analytics (UI & CLI)
- TensorFlow lite for microcontroller is always based on the code
available in 7.1 release
- CLI
- add [
'--quiet'][CLI_common_args] option to disable the display of the progress bar during the execution of the command.
- to generate a relocatable binary model, the
[
'--lib’] is no more requested, root lib directory is automatically detected from the installed pack.
'--range'option can be used with a simple argument to pass a simple value.- number of operations by data types is reported [(by layer and for entire generated model)][CLI_op_by_type]
- add [
- Core - Code generator
- different implementations of c-kernel have been improved to have
a better latency. Counterpart is to use more memory, and depending
of the used models and the expected options (allocate-inputs,..) the
activations buffer can be a little bit more important in comparaison
of the previous version.
- TensorFlow 2.9 and Keras.io 2.9 modules are used to import the
Keras (h5 file) and TensorLite file (tflite file) models
(
'tensorflow.keras'is no lore used).
- upgrade ONNX package to 1.10.2 version (no change for the ONNX
runtime 1.9.0)
- new layers:
- complete TreeEnsembleRegressor support (ONNX)
- QActivation, QBatchNormalization, QDense, QConv2D,
QConv2DTranspose, QDepthwiseConv2D (QKeras/Keras)
- QuantConv2D, QuantDense, QuantDepthwiseConv2D (Larq/KERAS). See the new article: [“Deep Quantized Neural Network (DQNN) support”][X_CUBE_AI_DQNN]
- enhance TimeDistributed support, wrapped layers: Conv2D, Dense,
Flatten, MaxPooling2D, ZeroPadding2D, Dropout (KERAS)
- improve the error message when a feature/operator is not
supported/implemented
- no more limitation of depth multiplier different than 1 for
depthwise quantized layers
- compression level (medium, high) can be applied for GEMM
operator
- add STM32G4/U5 series target for relocable binary model
- different implementations of c-kernel have been improved to have
a better latency. Counterpart is to use more memory, and depending
of the used models and the expected options (allocate-inputs,..) the
activations buffer can be a little bit more important in comparaison
of the previous version.
- Validation process
- add support for models which have the IO dimension shapes up to 6D (including the batch size)
Major bug fixes
- (bz122230) UI - fix report of the overall flasl/ram size in the
main tabl (multiple network UC)
- (bz125178) UI - clarify usage of the “report’s output directory”
user field
- (bz126575) UI - fix global memory footprint reported with
STM32U5 series
- (bz126177) UI - fix issue when changing the runtime from Cube.AI
to TFLM
- (bz121296) CLI - add STM32U5 series target for relocable binary
model
- (bz121296) CLI - fix “–range” option allowing 0.0 as min
value
- (bz123747) CLI - allow directory path name with spaces for
relocatable object generation
- (bz126042) Core - fix support of MEAN layer when not applied on
Channel dimension
- (bz122402) Core - fix import of LocalResponseNormalization as
lambda layer
- (bz130213) Core - fix support for depthwise quantized layer with depth multiplier different than 1
What is new in X-Cube-AI V7.1.0?
Enhancements and new features
- Enhancements of the User Interface
- adding new advanced setting interface to define the memory pools
- fix generation of the application template for the relocatable
binary model
- add multiple-IO support for the application template
- CLI
- introduce preliminary and optional option to pass a description
of the target to define the memory pools (see
[
'--target'][CLI_target_option] option)
- add free text entry to enter specific command line options
- introduce preliminary and optional option to pass a description
of the target to define the memory pools (see
[
- Core - Code generator
- add support for new layers:
- Normalizer, StandardScaler, MinMaxScaler, MaxAbsScaler, RobustScaler, RandomForest, ExtraTree, GradientBoosting, HistGradientBoosting, TreeEnsembleClassifier, ReduceLogSumExp, Scaler, TreeEnsembleClassifier, LinearClassifier, Where, Clip (ONNX-ML/ONNX)
- TFOpLambda, stateful GRU Layer (Keras)
- SPLIT_V, ReverseV2, SQUARED_DIFFERENCE (TFLite)
- [multi-heap support][API_multiple_heap] support allowing to split the activations buffer in different memory segments and to have first a better usage of the device with fragmented memory devices (no contignuous memory) like the STM32H7 series.
- add support for STM32 ARM Cortex M0 and ARM Cortex M0+
based
- upgrade TensorFlow lite runtime 2.7.0 and ONNX 1.9
- (bz100948) support of weights for the Keras custom layers
- add support for new layers:
- Embedded Inference API
- C-API break has been introduced to initialize the instance of the C-model (refer to [“API Breaking Change”][X_CUBE_AI_API_BREAK] article)
- report specific code error (
'AI_ERROR_CODE_LOCK') if CRC IP not accessible (bz110629)
- extend relocatable C-API to manage the CRC IP as shared resource
- Template, Validation and System performance built-in test
applications
- update generated code to use the new C-API (multi-heap, new
ai_bufferdefinition)
- improve code size (gain of ~20KB, toolchain dependent). The
default
'printf()'function implementation has been replaced by a low cost proprietary implementation.
- align the TFLM-c wrapper to be able to use the TFLM 2.7 runtime.
- update generated code to use the new C-API (multi-heap, new
- Embedded documentation
- add new article to describe the [API breaks][X_CUBE_AI_API_BREAK] with the rationale and to provide guideline/tips to limit the integration issues.
- update [“Embedded Inference Client API”][X_CUBE_AI_API] article
to describe the multi-heap support, introduction of helper function
to simplify the creation and the initialization of the c-model, new
'io_buffer'description for the N-dimensional tensor support.
Major bug fixes
- (bz114786) CLI - fix stm32ai CLI suppoprt in Collab/Jupyter note-book environment
- (bz103040/bz117764) Core - support for PACK layer with dimensions>4
- (bz90708) Core - support for unpack& transpose layer with dimensions>4
- (bz117202) UI - fix incorrect heap/stack size definition for
STM32H7 dual core projects
- (bz112369) UI - fix compuation of the requested arena size for
TFLM runtime
- (bz112369) UI - improve report of the unsupported operators for
TFLM runtime
- (bz111842) UI - close correctly the advanced settings window
- (bz108953) Core - improve support of ONNX LSTM operator (Now multiple outputs (final state, hidden state, cell state) for LSTM are allowed)
- (bz116529) Core - improve shared axes support in PReLU (support the case where 1 is present in the middle of input shape)
- (bz110221) Core - improve constant propagation for Pack and
Reduce operators
- (bz101344) Core - for ONNX model, sottmax not on channel axis is now supported by adding a transpose before and after softmax.
- (bz112224) Core - improve support of 2D ONNX MatMul operator with multiple inputs (second input not constant).
What is new in X-Cube-AI V7.0.0?
Enhancements and new features
- Enhancements of the User Interface
- enhance the STM32 development board setting. Insure that the clock system is correctly set by default for best performance.
- Core - Code generator
- Add support for ONNX integer arithmetic operators, i.e. mul/div/sum/sub for signed unsigned 8/16/32 bit formats
- Add support for new layers:
- Argmin/Argmax (ONNX – TFLite)
- ArrayFeatureExtractor (ONNX)
- Cast (ONNX - TFLite)
- LSTM (ONNX)
- SVM Classifier – SVC (ONNX)
- Unpack (TFLite)
- ZipMap (ONNX)
- Add partial support for new layers:
- TFLITE_SPACE_TO_BATCH_ND/BATCH_TO_SPACE_ND (TFLite): when generated from the conversion of Keras dilated convolution
- Add support to iForest ML ONNX operator
- Add support for new non-linearities:
- HardSwish
- Swish
- Extended support to:
- ReduceMean (ONNX) - Added support when applied to channel axis
- Mean(TFlite) - Added support when applied to channel axis
- Split (TFLite) layers - Added support when output tensor size on splitting axis is 1
- TFOpLayer – Added support to ceil, floor, LRN, reduce_min, rsqrt, slice, strided_slice operators
- Added check for tflite files
- Batch size information is now correctly propagated through layers in intermediate representation
- Improved identification of dimensions order for ONNX models
- Intermediate representation now uses the same channel position of the imported model
- Order of output of generated C code is now the same of the analyzed model
- TensorFlow runtime version moved to 2.5
- Modified the generated C code from ONNX models, in order for the user to pass data in channel first order
- Precision improvement for the quantized models in particular for the models which the scale factors close to zero
- Embedded Inference API
- Add optional user callbacks to manage the CRC IP as a shared resource
- CLI
- Relocatable - Add
--ihexoption to generate Intel hexadecimal object file - Improve check of the input validation data (shape/type)
- Add
--seedoption to set the initial seed for the generation of the random data
- Relocatable - Add
- Validation process
- Add two new metrics: bias/mean and standard deviation of the error
- Provide a Python module
ai_runnerto export an unified inference interface for the different X-CUBE-AI run-time: X86 or STM32 (including the TFLm runtime) through the aiValidation test application.
- Validation and System performance applications
- aiValidation: Add inference time per layer for TFLm runtime
- TFLM runtime
- Upgrade the source files with TensorFlow Lite for Microcontroller 2.5.0
- Embedded documentation
- How to upgrade a project with a new version of the library
- How to to run locally a generated c-model in C or Python environment
- Manage the CRC IP as a shared resources
- Add in TFLM article, a table to compare the supported operators between TFLM 2.5.0 and X-CUBE-AI
- Update the FAQ
- Complete/update the advices about the built-in validation flow
Major bug fixes
- (bz103986) Scalar activations are now correctly supported. An error is risen for scale equal to Infinite in quantized models
- (bz106312) Keras SimpleRNN is now correctly imported
- (bz108736) Fix potential bug about memory buffer corruption on
multiple output network models when allocate-outputs option is
enabled
- Fixed import of slice layer when size is –1
- Fixed support to multiple tensors produced by same layer and used in same layer
- Fixed merging of pad into multiple successive convolution layers
- Fixed support of ONNX Reduce layers with keep_dims=False
What is new in X-Cube-AI V6.0.0?
Enhancements and new features
- Enhancements of the User Interface
- add support of code generation with TensorFlow Lite Micro
(Validation, System Performance, Template)
- based on 2.3.1 git repository of Tensorflow
- add panel to add custom layer json configuration file
- add panel for external weight placement, UI + Automatically update scatter files or create it
- add checkbox to add the option –classifier for the validation (x86/stm32) (bz97448)
- enhance dual core (multiple context support) code generation
with MX6.1
- you can have one instance of X-CUBE-AI on the CortexM7 and one on the CortexM4
- add support of code generation with TensorFlow Lite Micro
(Validation, System Performance, Template)
- new operators/layers
- KERAS: Average, Custom layer, Lambda wrapper: tf.math.abs, tf.math.acos, tf.gather.. 25+
- ONNX: ConstantOfShape, DequantizeLinear, Equal, Gather, Greater, GreaterOrEqual, Identity, Less, LessOrEqual, Mean, Neg, Not, Or, QLinearConv, QLinearMatMul, QuantizeLinear, ReduceL1, ReduceL2, ReduceSumSquare, Shape, Xor
- TFLITE: EQUAL, EXPAND_DIMS, FILL, GATHER, GREATER, GREATER_EQUAL, L2_NORMALIZATION, LESS, LESS_EQUAL, LOGICAL_AND, LOGICAL_NOT, LOGICAL_OR, MIRROR_PAD, PACK, REDUCE_ANY, REDUCE_MAX, REDUCE_MIN, REDUCE_PROD, SHAPE, SQUARE, TILE, UNIDIRECTIONAL_SEQUENCE_LSTM
- Code generator
- add initial support for the Keras lamdda and custom layers
- add initial support of the Keras stateful LSTM layer
(batch-size=1 limitation)
- add warning messages for int/hybrid layers not supported
- improve error messages for unsupported-layers
- improve support for constant propagation
- improve prelu/relu integer support
- better support for generated TFLite model converted with TF2.3+
converter
- add new C-defines to know the dimension values by input/output
tensors (bz91718)
- add support to integer element wise functions
- add support to nested Sequential model in Keras
- generate new
<network>_config.hfile with the tool version definitions- run-time check of the TOOLS API is now strict, no forward/backward binary compatibility is considered
- add initial support for the Keras lamdda and custom layers
- CLI
- add new command (
supported-ops) to list the supported operators by Deep Learning Framework
- add new command (
- Validation process
- for the models with the inputs in integer, random data generator is now adapted to insure that the data are uniformly generated between [-128, 127] (or [0, 255] respectively).
- add new option
--rangeallowing to set the min/max values for the random data (default:[0, 1[) - add support to valid a Keras model with stateful LSTM layer (limitation: batch-size=1)
- add bool type support
- add code to support STM32 USB-CDC profile
- Validation and System performance applications
- add support for TFLm run-times
- Embedded documentation
- add new article about the TensoFlow Lite for microcontroller
support
- add new article about the Keras stateful LSTM support
- add new article to explain how to use the USB CDC profile for
aiValidation firmware
- update/rework the metric article to clarify the expected data
for validation
- remove section about the Qmn arithmetic support
- add new article about the TensoFlow Lite for microcontroller
support
Major bug fixes
- UI - fix dual core code generation with MX6.1
- UI - fix error when using using “Generate relocatable network”
in X-CUBE-AI UI with another name than network (bz96349)
- validation - fix order of the inputs/outputs for the
Keras/TFlite model with multiple I/O (bz101481)
- validation - enable support for model w/o weights and w/o activations buffer
- test applications - fix compilation issues with H7 DUAL core
(bz9060)
- test applications - fix compilation issue with Keil and -gnu
option (bz100215)
- enhance validation file importer to support only one sample by npz file (w/o batch dimension) (bz95755)
- fix problems with shape of RepeatVector and recurrent
layers
- fix TFlite L2_Normalization import
- fix bug on Conv2D float margin computation
- fix problem when scale bias layer is merged in convolutional layer with zero bias
- fix computation of complexity of dense
- fix scratch buffer shape computation for conv2d integer
- fix observer API to model with only one layer
- add support to multiple use of same activation tensors (bz72010)
- enhance eltwise optimization
- improve integer clip support
- fix ResizeBilinear TFLite op (half_pixel_centers parameter support for +TF2 version)
What is new in X-Cube-AI V5.2.0?
Enhancements and new features
- Enhancements of the User Interface
- add UI options and update the project generation to test and to
validate a relocatable binary model
- same level of features for the aiValidation and aiSystemPerformance test applications (only multiple networks is not supported in this case)
- GNU ARM Embedded tool-chain is automatically downloaded if not available
- add new UI button (Advanced Settings)
- define the user output directory for the generated files
(reports, data, ..)
- check box to allocate the outputs in the activation buffer
- define the user output directory for the generated files
(reports, data, ..)
- add UI options and update the project generation to test and to
validate a relocatable binary model
- TF Lite and Keras model support
- for the import and the validation of the TF Lite and Keras
models, TensorFlow 2.3.0 package is used.
- provide a better support of the TFLite models generated with TFLiteConverter 2.2 and later
- Keras.io support has been removed (TF_KERAS environment variable
is no more available)
- Keras NCHW models can be no more validated (code generation is always supported)
- Up-to Keras 2.4.0 models can be imported
- for the import and the validation of the TF Lite and Keras
models, TensorFlow 2.3.0 package is used.
- Inference run-time library
- performance improvement (with conv2D int8) wherever weights location (in internal or external flash)
- Code generation
- add new “generate” options to be able to generate a relocatable binary model - bz80560/bz80557
- for the split of the weights, each c-array is now prefixed with the name of the model to facilitate the data placement with IAR tool-chain. “static” keyword has been removed - bz89998/bz90000
- outputs buffers can be allocated in the activations/working buffer - bz89643
- Validation process
- add percentage of execution time by layer in the report for the validation of target
- add the computation of the L2r metric systematically
- add name/shape of the output tensor
- Validation and System performance applications
- re-work the source files to share the common functions between both applications and to avoid to mix STM32 specific code and the AI code.
- both are now fully based on the Platform Observer API
- no system heap is no more requested to use the aiValidation application test
- add support for relocatable binary model
- remove warnings for STM32L5 compilation with ARM Compiler 6
- Embedded documentation
- add new article for the relocatable binary model support
- add new snippet code for the usage of the Platform Observer API
- “End-of-process input buffer notification”
- “Dumping intermediate output”
- fix typo and mismatch with the current release.
Major bug fixes
- fix/improve support of TFlite reshape operator before FC operator (dim > 2) - bz93218
- add support to align_corners attribute of TFLite ResizeNearestNeighbor operator (TF2.3)
- improve the optimization step to remove the redundant conversions (code gen) - bz88996/bz92379
- (minor) reinforce the coherency check of the output types before calculation of the metrics
- fix ONNX importer for the reshape layer
- fix/improve memory allocator for specific corner case - bz88995
- (minor) report clear error when the output or workspace option is passed w/o argument - bz89157
- fix/improve reported information of the IO model (corner case)
- improve the execution time for the conv2d float kernel when the weights are located in the STM32 internal flash
- fix a bug in the final computation op for the optimized con2d pool integer kernel
- (minor) - fix decimal separator for reported time value - bz90001
- improve execution time of the clip nl operator - bz90289
- fix overflow calculation issue in the integer operation when scales values are closed to zero: < 10e-7 - bz90287
- UI - fix code generation in advanced mode (simplify overall files copy) + fix Makefile generation
- UI - fix keil generated project file for L5 (add DSP if not already there)
- UI - fix report of the metrics (multiple outputs case) - bz93608
- test applications - remove warnings for STM32L5 compilation with ARM Compiler 6
What is new in X-Cube-AI V5.1?
- Enhancements of the User Interface
- New graph to display the C-graph (operators and associated tensors)
- New graph to display the usage of the “activations” buffer
- C-Code generation / network runtime library
- Adding support to generate a c-array by weight/bias tensor
- Adding textual c-graph description (operators and associated tensors) in the reports
- Lighter network-runtime library support. Granularity of the inference kernel functions are aligned on the used integer scheme to decrease the final code size
- Improvement of the memory peak usage (RAM and ROM size)
- Improvement of the inference time of Convolution kernels (float and integer type) in particular when the weights are placed in a low latency memory device
- Embedded inference client API extension
- Adding platform observer API
- Validation
- Adding support for int8/uint8 validation files
- System performance application
- Adding executing time by layer
- Documentation
- Adding specific article for the quantization aspects
Major bug fixes and improvement
- adding ONNX Softmax, Hardmax, LogSoftmax, Resize operators
- upgrading subset of operators up-to Opset to 10 support of ONNX 1.6
- adding batch normalization and mul/add support for integer layers
- adding Keras simple RNNs support
- adding support for quantized concat operator
- removing system heap usage for recurrent layers
- fixing support for Keras GRU/LSTM/RNN layers when use_bias==False
- fixing support for Keras GRU/LSTM layers with non-default nonlinear function
- fixing ONNX shape interpretation (Concat and Slice) for 2D tensors
- fixing duplicated inputs for element-wise operators
- fixing support for TFLite/ONNX model with multiple IO
- fixing MACC calculation for ONNX GEMM layer
- improving parsing of TFLite reshape operator
- fixing parsing of Keras RepeatVector operator
What is new in X-Cube-AI V5.0.0?
- Support of ONNX floating-point network
- A subset of operators from Opset 7, 8 and 9 of ONNX 1.6 is supported
- Adding “per-channel” support for quantized model
- Enhanced support for Post-quantized and training-aware TensorFlow lite models
- Keras post-quantization process update
- Support of Mutiple IO network
- Model for multiple IO are now fully supported
- Bug fixes and enhancement
- Improvement of the RAM usage
What is new in X-Cube-AI V4.1.0?
- Support of TensorFlow Lite quantized network
- Support latest TensorFlow Lite quantized networks optimization, both floating point and integer quantized networks can be imported in the tool.
- Integer arithmetic for quantized model
- X-Cube-AI has full support for integer quantized networks allowing to optimize flash memory usage and inference time while keeping a good accuracy. Keras post training quantization tool also supports integer quantization.
- Support of external memories:
- The generated code can be configured to use external flash for weights or external ram for activations or weights.
- This allows to run bigger networks
- On ST STM32 boards the usage of external memories is fully plug and play
What is new in X-Cube-AI V4.0.0?
- Support of TensorFlow Lite in floating point
- Support of Keras network quantization
- Enhancements of the User Interface
- One click automated validation project build and run on the target
- New graph display
- New Logging window with cancel support that will give the results so far
- New command line interface allowing to perform the following
actions on a neural network
- analyze to give complexity, needed Flash and Ram size
- generate the C code
- validate on the desktop and on the target
- quantize using the min/max or greedy algorithm
What is new in X-Cube-AI V3.4.0?
- Bug fixes and enhancement in the user interface
- Support of additional Keras layers:
- DepthwiseConv1D: Depthwise 1D convolution
- SeparableConv1D: Depthwise separable 1D convolution:
- Better support of Linux and MacOS